Part Number: TMDSHVMTRPFCKIT
I am going to work on induction motor drive system and i want to buy HVACIMTR motor, but today when I checked ti website i found out it was not there for sale, does and body know where can I buy this motor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSHVMTRPFCKIT
I am going to work on induction motor drive system and i want to buy HVACIMTR motor, but today when I checked ti website i found out it was not there for sale, does and body know where can I buy this motor?
Please request your support:
I am currently working on a project to control the position of a three-phase induction motor with the KIT for sensored vector control and I need to know if I have to make some additional adjustments to use the kit with a motor of 1HP (746 W) 220 V and 60 HZ instead of the motor that usually comes with the kit which is 0.25 HP. Then I want to know what? and where ? I must configure the program or the hardware since the program of the code composer simply stops when the voltage of the VARIAC increases when I rise to more than 130 V the program stops but the engine continues to run.
I clarified that I connected the encoder and the motor correctly, I changed the encoder correctly in the software but still the program continues to stop and an error appears:
The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'. One of the FTDI driver functions used during the connect returned bad status or an error.
I also clarify that I have already modified several parameters of the file "settings.h", like the peak current and the motor parameters.
thanks for you comments.