Other Parts Discussed in Thread: DRV8305, , BOOSTXL-DRV8301, MOTORWARE, DRV8312, CONTROLSUITE, DRV8301
I am using the LAUNCHXL-F28069M with BOOSTXL-DRV8301 and DRV8305, and have the following questions pertaining to the use with Hall Effect sensors:
1. Is there a lab in motorware/controlSUITE that demonstrates the use of only Hall Effect sensors alone for control with the above boards? I was referred to one for the DRV8312 kit, and Lab 11E works with my boards, but only for start-up. Please advise with a lab #/example # using ONLY hall sensors with speeds of up to 5500 RPM for the eval board bundle I am using, if available.
2. In general, could one control a motor using this bundle kit, using only Hall Effect sensors, without any other sensor or sensorless assistance? I noticed that even the lab/code example for the DRV8312 kit used sensorless along with the hall sensors if I am interpreting correctly.
3. Is there a limitation, besides the use of 5V, for the type of Hall Effect sensor that can be used with the bundle kit I am using? For example; for the hall sensors, features like bipolar, latching, etc; is there anything required/incompatible in these regards?
4. I am also going to be driving a frameless motor, and will need to select and mount the Hall Effect sensors. Is there a limitation on the number of them to use, position, and angle? For example in many cases I see motors equipped with three sensors at 120deg apart. Is there an advantage to using more, placed at 60deg angles, or other configurations?