Hello,
I've noticed that when running the offset recalibration for the voltages at start-up those change with the value of the DC Bus Voltage applied (not like the current offsets which are constant). The inverter+motor pack that I am running is suppose to work with a big range of DC Bus voltages 200-700 V. Does this means that I have to run the offset recalibration every time I start up the inverter to acomodate for the different DC bus voltages? I would like to get rid of it to speed up the start-up time.
Kind regards,
Javier