Other Parts Discussed in Thread: MOTORWARE, DRV8301
Hi all,
I run the lab21 from motorware base on HVKit and F28069M. When I set "gMotorVars.Flag_enableSys" and “gMotorVars.Flag_Run_Identify" equal to 1, I just hear some noise, not any other reaction. I adjust the "
IPD_HFI_EXC_FREQ_HZ", but the result is the same. The motor I use is saliency: Ld=6.5mH, Lq = 9.5mH; Do I nedd more operation about this Lab?
I read the rotor position from the variable "angle_pu" in the debug window, is this right?
How to judge whether the lab operation successfully?
Thanks very much!
Eli