Other Parts Discussed in Thread: MOTORWARE,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. Yanming.
Yes, I connected AC power to P1 of HV-Kit.
I didn't connect probe of oscilloscope to HV-Kit.
I also know that HV-Kit is hot ground design.
As I explained attached file(tmds.pptx), I can't connect ISO emulator J1 of controlCARD to my computer
because of power-down of home electricity.
(I think this is short circuit when ISO emulator J1 of controlCARD is connected to USB port of computer)
Considering this condition, how this HV-Kit could be normal????
Hello, to many TI FAEs.
I want your decision for my problem as mentioned above.
I want exchange or repair this HV-kit.
Two and half months have passed since I requested solution for my problem to E2E community and TI service.
They continuously said that in order to exchange or repair my HV-kit, I should be confirmed from FAE at E2E community.
I posted my problem E2E community several times , but no one confirmed my HV-Kit is normal or not.
Who is responsible for exchange or repair for their product inside TI?
If there is no FAE's post for my problem, how can I solve my problem.
Hi Yongcheol,
You can find all documents related to InstaSPIN in the following fold if you download MotorWare ( http://www.ti.com/tool/motorware ).
"ti\motorware\motorware_1_01_00_18\docs\boards"
The default jump settings should work. The one thing you have to is inserting jump at [M3] J3 like below figure if you connect JTAG via J1 USB port in the ISO 06x controlcard.
I think the poor isolation is making your problem. The C71 in the controlCARD located between the isolation section to mitigate noise coupling, but sometimes it can make isolation issue. First of all, pls try removing this capacitor which is located on the back side of controlCARD.
Thanks,
Steve
Hi Yongcheol,
Sorry for wasting your time with EVM HW issue. I think you are here in Korea.
If you send it to TI office whose address is here, let me check it and get back to you.
주소:
서울특별시 강남구 영동대로 511 (삼성동) 무역센터 31층 텍사스인스트루먼트 코리아
임성일 이사
Tel: 02-560-6810