This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/INSTASPINUNIVERSALGUI: TMS320F2806

Part Number: INSTASPINUNIVERSALGUI
Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE

Tool/software: Code Composer Studio

Hi all,


I bought New Instaspin solutions High voltage kit for my new BLDC control drive development.

I got the Instaspin solutions kit with F2806x Control card, Now i want to connect this kit with HVMTRPFCKIT-BLDC-GUI (located inside controlsuite folder in Ti folder-C drive).

I am already installed controlsuite in my PC.

While i am trying to connect Kit with above GUI screen shows error attached in picture.

I am new for this.

USB cable connected and comport was detected in PC.

In control Green and Red LED was continuously glowing without any blink.

Help me how to solve this.

  • What controlCard are you using? F28069 or F28069M? This GUI can't support F28069M controlCard which it's better to be used with motorWare projects and GUI.

    You may refer to the "High Voltage Digital Motor Control Kit (R1.1) Quick Start Guide", need to load the target file into the controller first, and set the related switches to enable the onboard SCI to PC via the USB, and enable the codes to boot from flash.
  • Hi Yan,


      Can you tell the target file located where...? and how to load?

    I am using F28069M controlCard.

    I am using GUI composer located in motorware, while try to connect target from my PC it shows error. The error screen attached below

    Regards,

    Yuvaraj

  • Could you please refer to "GUI Quick Start Guide" in the folder of motorWare as below if you installed it? There is a detailed description on how to generate the .out file and use the InstaSPIN UNIVERSAL.

    C:\ti\motorware\motorware_1_01_00_18\docs\guis\universal