This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Startdelay in Position Mode

Hello guys,

i am using the Position Mode and i measured out the startdelay.

When i set the start command gMotorVars.RunPositionProfile = 1 it takes about 40 ms untitl the motor spins.

Attached Graph explaination:

When the SYNC = high then the gMotorVars.RunPositionProfile Variable = 1.

When RPM > 50 = high then Speed reaches 50 RPM.

Can you explain me why we sppend so much time?.

Thanks guys