• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » C2000™ Microcontrollers » All Tags » controlSTICK
Share
C2000™ Microcontrollers
  • Forums
  • Announcements
  • E2E Wiki

Browse by Tags

C2000™ Microcontrollers

Welcome to the C2000™ Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
controlSTICK
  • 28027
  • 2833x
  • ADC
  • bootloader
  • C Programming Language
  • c2000
  • CCS v3.3
  • CCSv4
  • cla
  • Code Composer Studio
  • controlsuite
  • digital motor control
  • DSP
  • eCAN
  • ePWM
  • eZdsp TMS320F28335
  • F28027
  • f28069
  • F2812
  • flash
  • I2C
  • piccolo
  • SCI
  • SPI
  • XINTF
Related Posts
  • Forum Post: Error connecting to the target on PICCOLO controlSTICK

    Miro Samek Miro Samek
    I can't connect to my PICCOLO controlSTICK. The Code Composer Studio gives the following error messages (one line for each attempt): Error connecting to the target: Error 0x00001200/-1135 Error during: OCS, Target, Unrecoverable emulation error Error connecting to the target: Error 0x00001200...
    on Jan 1, 2009
  • Forum Post: Re: TMS320f28335 FOC with motor control library

    vsi-pete vsi-pete
    Dear hello84, I suggest you try VisSim/ECD. It is a block diagram language for embedded control targeted at TI C2000 devices. It has a complete motor control block set that allows off-line simulation, automatic C code generation and CCS compile. It will select the proper TI motor control library for...
    on Apr 28, 2009
  • Forum Post: Piccolo PWM

    Mario Liebmann Mario Liebmann
    Hi all, I'm currently working with a Piccolo ControlSTICK to get a sin-waveform out of the ePWM module via a lowpass filter. Because this is my first microcontroller I'm programming I'm not used to the techniques. I'm stuck with setting up an interupt to change the compare value....
    on Oct 20, 2009
  • Blog Post: TI’s new C2000™ controlSUITE™ software provides comprehensive development package to accelerate each design stage of real-time control applications

    RandiW RandiW
    controlSUITE software: royalty-free software examples, libraries, application solutions and support Unlike traditional MCU offerings, controlSUITE software delivers the content and content management necessary to simplify evaluation, application adaptation, debug, test and reuse. Going beyond...
    on Jan 19, 2010
  • Forum Post: TI’s new C2000™ controlSUITE™ software provides comprehensive development package to accelerate each design stage of real-time control applications

    RandiW RandiW
    controlSUITE software: royalty-free software examples, libraries, application solutions and support Unlike traditional MCU offerings, controlSUITE software delivers the content and content management necessary to simplify evaluation, application adaptation, debug, test and reuse. Going beyond...
    on Jan 19, 2010
  • Forum Post: SWITCHING REGULATOR USING 28027USB

    salil desai salil desai
    HELLO I'M TRYING TO BUILD A SWITCHING REGULATOR USING THE F28027USB CONTROL STICK....I AM DRIVING A FULL MOSFET H-BRIDGE USING COMPLEMENTRY OUTPUTS FROM PWM1A AND PWM1B SINEWAVE PWM AFTER BOOTSTRAPPING...I'V IMPLEMENTED A VERY CRUDE SOFTSTART BUT IT WORKS...ONCE THE MOSFETS START SWITCHING AT...
    on Apr 12, 2010
  • Forum Post: ControlStick Stand-Alone Run?

    Qian Cheng Qian Cheng
    Hi, everybody I am new to TI's C2000 processor. There is no problem in runnig the example project of controlStick both in RAM and in Flash. But I want to let the controlStick run automaticlly. That is that after I plug the controlStick into the USB port, the processor can run the programme in...
    on Oct 12, 2010
  • Blog Post: Check out some of the buzz on the new floating-point Piccolo MCUs!

    RandiW RandiW
    Electronic Products’ video interview with TI’s Sang Chon really shows why TI is excited about the new floating-point Piccolo MCUs. Check out Patrick Mannion’s article and the contributed “Product How To,” which includes tips for leveraging the new Viterbi Complex...
    on Jan 11, 2011
  • Forum Post: Piccolo ControlStick F28069

    Verena Grifone Fuchs Verena Grifone Fuchs
    Hi, is there any detailed description on the F28069 USB controlStick hardware availabl? I need the header pin diagram of the controlStick to connect to my hardware design. The only thing I can find is the header pin diagram of the F28027 in the "one-day workshop"-lab pdf. Is it pin...
    on Apr 26, 2011
  • Blog Post: TMS320C2000 Piccolo Hands-on Multi-day Workshop - Dallas, TX - March 16-18, 2010 **Registration is open! **

    Beth Rea Beth Rea
    The TMS320C2000 Piccolo multi-day workshop is a hands-on technical course facilitated by qualified Texas Instruments' instructors. This workshop will cover the Piccolo F2803x devices, which are the latest members of the C2000 MCU family. The workshop steps the user through system initialization...
    on May 28, 2011
  • Forum Post: TI ControlStick Maximum Ratings

    Tobias Gro��e-Puppendahl Tobias Gro��e-Puppendahl
    Hi, unfortunately I couldn't find a datasheet regarding the TI ControlStick. Thus, I was wondering if there are maximum ratings for the current through the 3V3 pin? Moreover, may a short circuit between 3V3 and GND pin lead to any damages? Since I connected the control stick to my custom electronic...
    on Jul 13, 2011
  • Forum Post: I2C without interrupts, simplest Tx

    Toby Mole Toby Mole
    Hi Folks (F28027 ControlSTICK) I am trying to implement a very simple I2C transmit via I2C, currently with the following code execution hangs forever waiting for I2CSTR.bit.XSMT to become 0. The spec says I2CSTR.bit.XSMT should become 0 after the byte in the I2CDXR has been sent, is this correct...
    on Oct 12, 2011
  • Forum Post: ePWM Event Trigger SOC A/B ?

    Toby Mole Toby Mole
    Hi There (F28027PT piccolo ControlSTICK) I am getting confused with the A/B designations used for the names of SOCs/ ADC channels and ePWM Triggers. I have set SOC0 to ADC A1, SOC1 to ADC B1 and SOC2 to ADC B2. They are all set to be triggered by ADCTRIG9 (ePWM3, ADCSOCA) However I wish...
    on Feb 14, 2012
  • Forum Post: Piccolo standalone operation

    Toby Mole Toby Mole
    Hi Folks Is there a guide for setting up the piccolo controlStick to run code from flash without using CCS to tell it to boot? (i.e. plug in the Stick and it boots the code already in flash) I found several online, but they seem to be for older versions of CCS, I am using 4.2.4.00033 Thanks
    on Feb 14, 2012
  • Forum Post: Multiple ADCINT1 & 2 in PIE vector table??

    Toby Mole Toby Mole
    Hi again folks (F28027PT Piccolo ControlSTICK) Im setting up EOC interrupts for the ADC and notice there are multiple entries for ADCINT1 and ADCINT2 in the PIE vector table at INT1.1, INT10.1 & INT1.2, INT10.2 respectively. Are they the same interrupts? what is the reason for this? Thanks
    on Feb 14, 2012
  • Forum Post: 28069 controlstick

    Calum Mackinnon Calum Mackinnon
    I have a customer with the following errors Can you help? I’ve purchased the controlstick 28069 , try to debug and get the following messages. C28xx: Flash Programmer: Missing Flash Programming Settings. C28xx: Flash Programmer: Error erasing Flash memory. C28xx: Flash Programmer...
    on Mar 28, 2012
  • Forum Post: Rewire SCI on control Stick

    Toby Mole Toby Mole
    Hi There If I was to disconnect the FT2232D from the SCI port to use the port for something else, will the CCS4 IDE still load and debug the code on the controlSTICK? Am I right in assuming it uses only the JTAG for this functionality Thanks. (F28027)
    on May 1, 2012
  • Forum Post: [F28027] SOCFRC causes fail during ADC offset self cal

    Toby Mole Toby Mole
    Hi I have copied the adcOffsetSelfCal() and its dependent functions from the piccolo example files and is called when I set up the ADCs for use after device initialisation and before my main loop starts. However in the function adcConversion() the SOC 0-7 are initially forced to start the "ping...
    on May 16, 2012
  • Forum Post: INT1.1 & 1.2 vs INT10.1 & 10.2 and PieVect.h

    Toby Mole Toby Mole
    Hi there Is there a way I can override the struct created in the PieVect.h common header file? I have currently altered it because I am using ADCINT1 & ADCINT2 in PIE Group 10 instead of 1 after I spent ages trying to figure out why my ADC interrupt was causing an ITRAP. It would be great to...
    on May 30, 2012
  • Forum Post: piccolo controller F28069 control stick

    chakravarthi g chakravarthi g
    The problem i am facing is when i am executing the example given in the path c:\ti\controlsuite\device_support\f2806x\V130\F2806X_examples\sci_echoback when i import the project into the css i am getting an error as below The managed make project file error: error loading managed make project...
    on Dec 10, 2012
  • Forum Post: F28069 SPI with Interrupts and no FIFO

    Emanuel Eni Emanuel Eni
    Hi everybody, I have to do a project with SPI on a piccolo controlstick with SPI . I need the piccolo as a master. I want to use the SPI with interrupts, but I don't want to use the FIFO buffers, since the communication should have the latest data. In my opinion I don't need the extra FIFO...
    on Mar 1, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use