Welcome to the C2000™ Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q:
Do we have any document describing migration from the C24x CPU to the C28x?
A:
We have information on migrating code from a 24x core to the 28x core. It is in appendix B and C of the TMS320C28x CPU and Instruction Set Reference Guide www.ti.com/lit/SPRU430
One thing to note is the 28x is a much better C engine then the 24x was. I think many customers that have gone down this route in the end just rewrote things in C.
Apart from the core change, there are many differences between the 240x & Piccolo (Operating frequency, package, Supply rails required, Presence of onchip POR/BOR/VREG/internal-oscillators etc etc). Even on peripherals that exist on both devices (SCI/SPI) , there are differences like presence of a FIFO.