This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Differences in clocking for USB between RM48x and RM46x Hercules MCUs

There is a slight difference in the way the clocks are configured to the USB host/device modules on the RM48 versus RM46 MCUs.

RM48x:

RM46x:

As shown in figures above, on RM48x you need to configure VCLKA3 (same as VCLKA3_S) to be 48MHz for the USB device/host, and then configure the VCLKA3_DIVR to be divide-by-4 to get the 12MHz required by the USB host.

On RM46x, you need to configure VCLKA3_S and VCLKA3_DIVR such that the VCLKA3_DIVR is 48MHz. Then there is a hard-coded divide-by-4 which generates the required 12MHz clock signal for the USB host.

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.