This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMS570LC4357: Can we downloaded the firmware via CANbus or Ethernet port for TI MPU tms570lc4357?

Expert 4565 points

Replies: 3

Views: 152

Part Number: TMS570LC4357

Can we downloaded the firmware via CANbus or Ethernet port for TI MPU tms570lc4357?

  • Guru 54135 points

    Hello Ken,

    Yes, the data can be downloaded to MCU flash through CAN/UART/Ethernet bootloader. But the bootloader itself has to be programmed to MCU flash through JTAG.

    Those bootloaders can be found in ti.com, For example:

    Thanks and Regards,
    QJ Wang

  • In reply to QJ Wang:

    QJ,

    Thanks for reply. What is the downloading rate via CAN or Ethernet?

  • Guru 54135 points

    In reply to Ken Yeap76:

    Hello Ken,

    For CAN, you can use any baudrate to download to download the code, but upto 1Mbps (CAN protocol).
    For ethernet, we support both 10Mbps and 100Mbps.

    Thanks and Regards,
    QJ Wang

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.