Hi.
RM48L950
Pin numbers of K16, L16, M16, N16, U12, V12, W12, T11, U11, V11, W11, T10, U10, T9, U9, U8, U7, U6, U5, T4, J4, T3, U3, V3, T2, D13, A15, B15 and B16
are NC(No Connects) by SPNS174 of Figure 2-4(11 page).
But, the SPANS174 of Table 2-45 is not written.
What's Corrected..?
Since they are no connect (NC) pins, we did not put it in Table 2-45. Both are correct.
Regards,
Haixiao