Greetings,
I need more serial ports on the RM48 and I was wondering if the N2HET pins can be configured for UART communication. I found an application note SPNA097 from June 2006 that presents a UART implementation using the High-End Timer on the TMS470. However I have not seen a similar application for the RM48/TMS570 MCUs. I haven't looked at the implementation closely yet, so at this point it is not clear to me if the sample HET code will work on the RM48 and how the code needs to be modified for the RM48's higher clock frequency.
Has anyone done this, can you provide some sample code for the RM48 ?
Thanks,
Marius