Hi everybody,
I apologize because this kind of conversation is old, but I need to find out a demo for the CAN bus.
I'm using a TMS570 MCU in the Hercules Development Kit with CCS v5.
Can someone help me?
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everybody,
I apologize because this kind of conversation is old, but I need to find out a demo for the CAN bus.
I'm using a TMS570 MCU in the Hercules Development Kit with CCS v5.
Can someone help me?
Thanks in advance.
Hi Luigi,
Enclosed please find the HDK test code which include DCAN1 and DCAN2 communication function. You need to wire CAN1 H/L to CAN2 H/L.
Regards,
QJ
Hi,
unfortunately the software doesn't work.
The CCS says this thing during the debug session:
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_svc ./src/sys_intvecs.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "TMS570 HDK RevE BE32.out" not
>> Compilation failure
built
gmake: *** [TMS570 HDK RevE BE32.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
What can I do?
Is this the demo software?
Thanks.
Hi Luigi,
Please make sure you have cmd file in the project. I just compiled the project without any problem.
Regards,
QJ
Well,
I think that the TMS570LS3xFlashLnk.cmd is inside the project.
I "Import" the project inside my CCS workspace wdirectly from your zip file.
I don't try TI V5.0.4. Can you please try TI V5.0.1? I will download 5.0.4 and try it later.
Regards,
QJ
Check sys_svc.asm in the src folder. It is probably checked as "Exclude from build"