Hi,
I'm working with a RM48HDk and need the maximum performance from one of the HET.
In Halcogen I've set the VCLK2 prescaler to 0 obtaining a HET HR clock of 200MHz.
That's the double of default frequency but my het program works well (and reach the performance I need)
Can this set be dangerous for the HET ?
Grazie,
Matteo
p.s:
This info should be on SPNS174A but for some reason the table on par3.3 is uncomplete. Do the docs has been updated?