This question was posted previously here but not answered to my satisfaction:
http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/203000
I am using HALCoGen to generate source code for the RM48L952ZWT.
reg_esm.h contains the following:
typedef volatile struct esmBase
{
uint32 EEPAPR1; /* 0x0000 */
uint32 DEPAPR1; /* 0x0004 */
uint32 IESR1; /* 0x0008 */
uint32 IECR1; /* 0x000C */
uint32 ILSR1; /* 0x0010 */
uint32 ILCR1; /* 0x0014 */
uint32 SR1[3U]; /* 0x0018, 0x001C, 0x0020 */
uint32 EPSR; /* 0x0024 */
uint32 IOFFHR; /* 0x0028 */
uint32 IOFFLR; /* 0x002C */
uint32 LTCR; /* 0x0030 */
uint32 LTCPR; /* 0x0034 */
uint32 EKR; /* 0x0038 */
uint32 SSR2; /* 0x003C */
uint32 IEPSR4; /* 0x0040 */
uint32 IEPCR4; /* 0x0044 */
uint32 IESR4; /* 0x0048 */
uint32 IECR4; /* 0x004C */
uint32 ILSR4; /* 0x0050 */
uint32 ILCR4; /* 0x0054 */
uint32 SR4[3U]; /* 0x0058, 0x005C, 0x0060 */
uint32 ESTATUS5EMU; /* 0x0064 */
} esmBASE_t;
The RM48x TRM does not list SR4[2-1] nor ESTATUS5EMU. Where can I find documentation on the function of these registers?
Thank you,
Ryan