We are in a process of designing a system based on TMS570LS3137.
The system will have external SRAM and FLASH memory interfaced in addtion to available internal memory.
As per requirement, we may have to execute the Code from external SRAM connected to EMIF interface.
Is it possible to on TMS570LS3137 (Cortex R4F) to execute from external RAM.?
Also would like inputs on whether such a implementation(executing from external SRAM) would have any benefits/drawbacks over execution from internal memory RAM/FLASH, besides additional memory that can be interfaced.