Sirs,
Is it possible to set BITERRFLG=1 when all the following condition meet?:
- SIMOFUN[1]=1, that is, MIBSPI1SIMO[1] used.
- But the PINMMR14[1]=0, that is, MIBSPI1SIMO[1] not used.
- Pin#106 have 3.3 volts.
- MIBSPI1 starts in 4-wire mode as master.
The part# is TMS57021xxCPGEQQ1.
My customer reported MIBSPI1.SPIFLG.BITERRFLG=1.
The BITERRFLG bit description in the TRM didn't explain our case. SIMO transitions fast and is stable at the half clock later.
But when we disconnected 3.3 volt pin #106, the phenomenon stopped.
Therefore we are intersted in the PINMMR14[1] and MIBSPI1SIMO[1].