Hi,
when do you plan to release the HALCoGen for FreeRTOS 8.2.0?
Or can I make my own changes in the files which are created by the current version of HALCoGen which supports FreeRTOS 8.1.2? The reason is that the code crashes when I use the new feature in FreeRTOS 8.2.0. - task notifications. I don't know the reason but it happens in this macro:
os_portmacro.h:
#define portYIELD_WITHIN_API() { portSYS_SSIR1_REG = portSYS_SSIR1_SSKEY; asm( " DSB " ); asm( " ISB " ); }
The strange thing is that it crashes the SECOND time it is executed.
Maybe you already have some working code which I could use (before the new HALCoGen release)?
Kind regards,
Lars