Hi. We are using the Hercules RM48L952ZWT board. If we set in HalCoGen, that we want to use Terminal M17 M17- EMIF_nCS[4]/RTP_DATA[7] as GPIO. Under the HalCoGen RTP tab, we can see where to set RTP_DATA[7] to a GPIO.
1. In PINMUX M17 terminal tab, do we want to select the RTP_DATA[7] so it is used as GPIO as we configured in RTP, or do we not select anything for it to work as a GPIO.
2. In the software how can we get to this pin to change it's settings to 0 or 1? Is there an initialization function that needs to be run so the HalCoGen settings as this terminal M17 us being GPIO is executed at poweron and it is the default as we configured in HalCoGen?
Thank you