Hi,
I saw that the new release of HALCoGen (04.03.00) includes support of FreeRTOS source code generation.
Unfortunately I tried to recompile my project with it and it did not work.
After investigating, there are some bad initialization variables in the file TMS570LS1224PGE_FREERTOS.cnf
Actual values:
VAR.FLASH_BANK_LINK_BASE_ADDRESS_0.DEFAULT=0x00000020
VAR.FLASH_BANK_LINK_LENGTH_0.DEFAULT=0x0013FFE0
Correct values:
VAR.FLASH_BANK_LINK_BASE_ADDRESS_0.DEFAULT=0x00008020
VAR.FLASH_BANK_LINK_LENGTH_0.DEFAULT=0x00137FE0