Hello,
We have problem to flash TMS570xxxxx (LS3137 and LC4357) with UniFlash tool. Problem is caused by POM unit (parameter overlay module).
POM is activated by SW and Uniflash didn't disable POM. With enabled POM it is not possible access/program flash memory at overlayed addresses. Therefore Uniflash fails with this messages:
[12:43:16] ERROR >> CortexR5: Error during Flash verification (Flash algorithm returned error condition). Operation cancelled. [12:43:16] ERROR >> CortexR5: Flash verification returned error condition. Operation cancelled. [12:43:16] ERROR >> CortexR5: GEL: File: abcdef.hex: Load failed. [12:43:16] File: abcdef.hex: Load failed.
Is it some work-around to modify init before programming? It mean add sequence to disable POM?
Jiri Dobry
PS: messages are litle strange. It indicate problem on verify stage, but it fail during erase verification.