how many PWM outputs can be generated using NHET from TMS570LS3137 series and RM48L series MCUs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
how many PWM outputs can be generated using NHET from TMS570LS3137 series and RM48L series MCUs.
Thank you Mr.vineeth,
this is the first time am steeping in to hercules controller and programming also. please help me with some sample program with and duty cycle. i will alter it based on my need.
Thanks and regards
K.Manjunatrhan
Hi Manjunathan,
You can use HALCoGen tool to get started on Hercules development. HALCoGen provides a graphical user interface that allows you to configure peripherals, interrupts, clocks, and other microcontroller parameters. Once the device is configured, you can generate peripheral initialization and driver code, which can be imported into CCS, IAR Workbench, or Keil uVision. This tool has a blackbox driver for the NHET which lets you create at most 8 PWMs (with variable frequencies). But since you need 32 PWMs, you can select the option to write your own driver for the NHET. You can then use the HET IDE to write the NHET driver suited for your use. The HET IDE has sample NHET code to help you ramp up. It should be fairly straight forward since you want PWMs with constant frequencies. If you face any issues, please don't hesitate to write back.
Thanks and Regards,
Vineeth
Thank you Mr.vineeth.
I will fly back to you if i had any struggle.
thanks and regards
K.Manjunathan