I'm using a TMS470M hercules board to sense a digital signal. When switching boards I noticed that the gio pin on my new board does not fire an interrupt when my signal goes high. Is this a hardware issue or can the board be debugged?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using a TMS470M hercules board to sense a digital signal. When switching boards I noticed that the gio pin on my new board does not fire an interrupt when my signal goes high. Is this a hardware issue or can the board be debugged?
When we drive the gio pin as an output logical high, the pin's voltage stays at half the rails. So when we power the board at 5V using the usb supply, the pin outputs 2.5V. Does that provide any clues for the diagnosis?
Hi,
First, I scanned through the HDK user guide () and I do not see any mention of support for powering the HDK board from USB. Please only use the provided power supply or another 5v to 12v power supply connect to the barrel connector labelled P1.
What are the amplitude of the inputs you have connected to the GIO which is not working?
Regards,
Karl