Hi,
I am using the TMS570LS0332, and am confused about the amount of flash space available. The TRM (spun 517a) indicates 384 KB of flash, but then notes that sector 14 (128KB) "is not accessible or included in the TMS570LS03x configuration"
The Halcogen generated linker file for the 0332 shows a length of (0x60000 FLASH0 + VECTORS), which would be 384KB of flash.
I get an undef exception if I try to use the flash api to calculate the checksum up to 0x0005FFE0, but it is fine if I run it up to 0x0003FFE0.
Am I missing something, or is the TRM correct, and Halcogen is generating a linker file with an incorrect length? I am using Halcogen 4.4
Thanks,
David