In working with the FEE module I eventually found the example FEE example application that is included with the HALCOGEN stuff. I followed the directions at the top of the file in order to get it running and have been able to get it to compile and run but the FEE module never gets properly initialized and as a result hangs at the top of the program where it checks for initialization prior to proceeding. The module never seems to make it out of UNINIT status. I have been unable to trace down where I went wrong but it seems like something isn't configured right. I have included the CCS project that I am using for this test application. The F021 libraries, files, and HALCoGen files are all located in the HALCOGEN folder in the project.
I am using a TMS570LC43x development kit for my project and HALCoGen v. 4.04.00, and CCS 6.1.0.00104.