The interrupts are configured on IRQ with HCG:
The IRQ interrupt is enabled
The IRQ flag is ON in the ECMP instruction of NHET program:
We can see that the data field of ECNT instruction is higher than the data field of ECMP instruction. So an interrupt should be rise.
Here we can see that the Offst1 is correct, the interrupt is enabled and the interrupt flag indicates the interrupt occurs. But the vector interrupt is not fetched and the interrupt routine doesn’t start.
What is missing?
Thanks for your Help
Jerome