Hi there,
I have completed a prototype development which MCU is RM48L952. Right now I want change the MCU to RM44L520 which is pin to pin with RM48L952. The hardware have been completed and past the test.
My question is
1. is there any simple way to migration from RM48 to RM44
2. I used HALCoGen 04.04.00 to generate the code for RM48 before. Is there any simple way to migrate code by set up the HALCoGen tools.
3. If I have to re-write the code or re-build a code by HALCoGen?
Thanks,
Dison