Hi TI,
I am working with N2HET and HTU of TMS570LC4357. And I am using F-ree RTOS driver code from HalCoGen.
I want my HTU Module to transfer data from Main RAM to N2HET RAM Location when trigger is given by one of the instruction written in N2HET RAM.
To achieve this, I did configuring N2hET, HTU Module only once in the 10ms Task. After that N2HET will do toggling a pin with certain intervals defined by the data that HTU Transfers to N2HET RAM.
So in my code I follows the following approach and I cannot achieve achieve the concept.
I don't know why it is happening? Please anybody explain me about this.
And To overcome this I just tried in the following way.
So please explain me why these two things happen?
(At the time of writing this post, I examined again and I noticed that I cannot update even a single bit of a register associated with the HTU Module after RTOS Code is run.)
I cannot find anything meaningful from these scenarios. Please anybody help me in understating.
And how to Stop and Reset HTU/N2HET Module and re-configure it while it is working with any other configuration.?
Thanks in advance,
Regards,
Karthikeyan.K