Hello.
First the current setup:
I connected the USBmini port with a USB Port of a PC.
Then I connected an XDS220 Adapter to the JTAG header on the RM42 or RM48 board(I have both boards).
Over the XDS220 I want to flash the µC, and over the USBmini I want to communicate with it.
Now the question:
Is it possible to let the XDS220 connected on the RM4x board, AND let the USBmini cable connected to the RM4x board at the same time?
My problem is, that when the XDS220 the USBmini are connected to the board, the flashing over XDS220 is not possible.
Neither over USBmini nor over XDS220.
Do I need to disconnect the onboard XDS100 emulator from the rest of the board to be able to flash the µC over XDS220
Regards:-)