This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS12x SPI MAXCLOCK?

I want to use this microcontroller, but i want to know which  MAXCLOCK SPI or MAXCLOCK SSI  that i can configure,i want tho use a SPI memory ( that work at 108 MHZ in single mode) to save the raw data(bits) of a image sensor(that works at 6MHz to 96MHz), so i need to know the MAXCLOCK limit of this microcontroller

  • The maximum SPI clock supported by the TMS570LS12x devices is 25MHz as shown in Tables 7-35, 7-36. 7-37, and 7-38 of the device datasheet foTMS570LS1225, SPNS191B. The mac SPICLK limit is specified as a minimum cycle time of 40ns in each of the tables. Each table is specific to a specific SPI configuration (Master/Slave, Clock Polarity, Phase).