In TMS570LC4357 uC, What will be the max speed of RTP and DMM Interface?? in the Datasheet, Page No: 151 & 153 - DMM & RTP Clock mentioned 110Mhz as Min. Then what is the max clock speed? pls reply...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In TMS570LC4357 uC, What will be the max speed of RTP and DMM Interface?? in the Datasheet, Page No: 151 & 153 - DMM & RTP Clock mentioned 110Mhz as Min. Then what is the max clock speed? pls reply...
Hello,
Take RTP for example, the datasheet uses the parameter tcyc(RTP) to specify the minimum cycle time of 9.09ns or 110MHz. 9.09ns is the minimum clock period which is also the maximum frequency (110MHz) at which the RTPCLK can operate.