Dear community,
I've an RM57Lx LaunchPad and one HDK. Previously the Launchpad and the HDK worked fine. Unfortunately, the Launchpad cannot be connected since this noon after the lunch break.
I was debugging a simple tutorial project on the launchpad with IAR EWARM IDE and another simple tutorial project on the HDK with CCS v6.1 at the same time. The Launchpad and HDK were connected to my laptop via a USB hub SSK:SHU028 (with 5V adapter).
Before the lunch break, I had stopped debugging on both devices (LaunchPad and HDK) but I only plugged out the LaunchPad from the USB hub whereas HDK remained connected to my laptop.
After lunch break, I plugged in the launchpad to the USB hub:
The XDS110 status LEDs (LED7, LED8) lighted up for about one second then died out. After that, the launchpad cannot even be connected to other PCs in the lab.
Can the launchpad be reset?