Hello All,
I am using rev. D silicon. I have peripherals on the SPI1 and SPI5 interfaces in which I don't have a SPI mode problem/issue.
The DS3234N RTC says it is compatible with Modes 1 and 3. I could only get Modes 0 and 2 to work on the SPI3 bus.
I have put a serial decoder on SPI3 and it looks fine in Modes 0 and 2. The RTC receives commands and responds to read requests.
Has anyone seen an issue like this? I reviewed the errata for Rev. D of this silicon and if I understand correctly; the errata only applies if the 3137 is a slave on SPI3.
Thanks In Advance,
John W.