Hi,
I'm evaluating a TMDX570LC43HDK with respect to replacing our existing TMS570LS3137 design.
Whilst porting our existing bootloader and application firmware I observed some strange behaviour with the nError LED and CCS whilst trying to debug.
To simplify matters I created a build of the rtiBlinky project using HALCoGen 04.05.01 which I have attached.
1) When I debug this on the TMDX570LC43HDK the nError LED is off the first time the code is run. If I pause the code the restart button in CCS is greyed out as shown here shouldn't this be available?. If I add a breakpoint to the code and run again when you hit the breakpoint the restart button is now available as expected.
2) After hitting the breakpoint if the restart button is pressed the code resets and the nError LED is now on, why as this has now reinitialised the device based on the HALCoGen code?
3) If I create a release build of the rtiBlinky project and program the TMDX570LC43HDK when the power is removed from the board and plugged back in the nError LED is always on, this does not look right can you explain this behaviour?
I'm using:
HALCoGen 04.05.01
CCS Version 6.1.1.00022 with all the latest updates installed.
Please help explain this behaviour?
Kind regards,
Stu