Hello. I'm trying to make a programmer for an MCU TMS570 based on another microcontroller.
The idea is to make a system which can update the firmware in a TMS570. I'm trying to avoid using a bootloader.
What possibilities do I have to make that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. I'm trying to make a programmer for an MCU TMS570 based on another microcontroller.
The idea is to make a system which can update the firmware in a TMS570. I'm trying to avoid using a bootloader.
What possibilities do I have to make that?
The only supported method for programming a TMS570 device without a boot loader is through JTAG and the F021 Flash API. Take a look at these two items: SPNA230 and F021 Flash API.