I am a rookie with this launchpad.
Recently I have been working with ADC, however problems occur.
1, It seems the ADC can only convert voltage below 2V or so. if I supply bigger voltage, it will be stuck in the code "while((adcIsConversionComplete(adcREG1,adcGROUP1))==0);"
I don't know why.
2, Is there a formula for the adc output value and the input voltage?
The adc outputs are around 3000, which confuses me.
Thanks