Hi, during test FEE,I set two virtual sectors and only one block on virtural 1.And I can write data to the Flash,and verify by debug tool Memory View ,all the data is ok.
like below,the write API is :
TI_Fee_WriteAsync(1,*wrbuf)
I set block size as 24 bytes ,data select bits as 0,and number of 8 bytes write as 3
After I succeed write the data, I want to read the data back,so I use
TI_Fee_ReadSync (1,0,*rdbuf,24)
But I read data always is the data I write last,which mean I can not read the data I write at the first or the second,only the last one
So I want to know how to read all the other data back?