According the tech manual, the 43X MCU has two banks of flash that are 2MB in size. Is there a way to change which bank is used as the program boot location? We are looking at an application where we want to update the software in the field without access to the JTAG. What would be ideal is an external pin that could be used as a bank selection.