I was thinking on using the application note: http://www.ti.com/lit/an/spna228/spna228.pdf which uses the N2HET assembler IDE. The encoders give 1440 pulses per
revolution and the motors work at 11RPM. Here I have one question:
- Do I need to configure something on the HALCogen fot the N2HET to work properly? Or with the configuration on the IDE is enough?
I saw this post https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/305646 which uses the HALCogen Edge Detect configuration. Would it be too difficult to
modify the source and the include of the N2HET to male it work with the 22 pins? How the HETDIN register works??
Is there any other way to use the N2HET pins to get the encoders data?
thanks and best regards