Hi,
we are using the Safety library demo application of TMS570LS0432. We are facing a problem with enabling the Flash Wrapper Diag Mode 5 Test on startup. The code for this is commented by default in demo application for some reason. When we try to include this code, micro controller reached to prefetch abort state. We are not able to do debug this issue. What could be the problem?
The following is the code which is commented out by default.
#if 0
/* Run Address tag mode test on Flash */
retVal = SL_SelfTest_Flash(FLASH_ECC_ADDR_TAG_REG_MODE, TRUE, &failInfoFlash);
INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
#endif
Thanks & Best Regards,
Sreekanth Reddy Challa