Hi,
I would like to generate the esm low level interrupt group 1 channel 26 (SRAM EVEN bank correctable interrupt). I am using the below function provided by SafeTI library to generate the interrupt. I have configured ESM properly to generate the interrupt.
SL_SelfTest_SRAM(SRAM_ECC_1BIT_FAULT_INJECTION, TRUE, &failInfoTCMRAM);
When i run the above function, the SERR bit in the RAMERRSTATUS register sets to "1". Still i do not get the interrupt. I am in debug mode.
Does being in debug mode fails to trigger interrupt?
Thanks & Best Regards,
Sreekanth challa