Hi, I'm new to Hercules and Embedded Development. I'd like to debug with CCS when ECC is burned and ECC function is enabled Using HALCoGen.
I'm not good at English, Please forgive the poor English of the question.
I'm using
・TMS570LS3137 HDK
・CCS v5.5
・nowECC v2.17
・nowFlash v3.42
Step 1
I made a program that is ECC function enabled and built the program(a.out).
Step2
I tried to debug with CCS(XDS100v2), but cannot debug.
TMS570LS3137 HDK' D1 RED LED(ERROR Signal) is lighted and did not come main() in CCS.
↑
I thought this problem was caused by not buring ECC, still enabling ECC function.
Step3
I used nowECC and nowFlash, generated ECC(a_ECC.out) and burned ECC to HDK.
It seems to be worked fine. But I want to debug this with CCS.
Note : I used this nowECC' command [nowecc -i a.out -f021 16M_ADD -r4]
How to debug with CCS, when ECC enable.
Can someone help me?