Hi there,
I got the demo to work and was just testing its behavior among different scenarios. One of them is starting the system without an ethernet cable plugged in the ethernet port.
In this configuration, the demo serial output is:
DEBUG - Getting PHY ID....SUCCESS
DEBUG - Getting PHY Alive Status...SUCCESS
DEBUG - Getting PHY Link Status...!!! ERROR !!!..DONE
-------- ERROR INITIALIZING HARDWARE --------
NOTE: if I connect the ethernet cable to a PC with the wrong IP and network/netmask, it is still able to initialize the hardware.
Is this how it is supposeto work? Or the demo doesn't have the feature to initialize the interface without an actual connection?
Best regards,
Julio