HI,
I am trying to download program though uart port on tms570lc4357, but i can not get any example or user guide. could any one tell me how to do.
however, the resource spna193.zip is for other series chip. Can i learn from that.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I am trying to download program though uart port on tms570lc4357, but i can not get any example or user guide. could any one tell me how to do.
however, the resource spna193.zip is for other series chip. Can i learn from that.
Thanks.
Hi Charles
Thanks a lot. According to what you said and the spna193.pdf , i am trying to port the project to LC4357 which is used for LS31x device.
I got some problems. Here attachment is my project in ccsv6.2.
1. in flash_definitons.h file, how to define flash sectors? The flash memery in lc4357 is larger than lsxx.
2. define SYS_CLK_FREQ as 300 is right?
3. which F021 api lib is for lc4357?F021_API_CortextR4_BE or F021_API_CortexR4_L2FMC_V3D16.
4. here is my cmd file. Is that right?
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000014E0
FLASH0 (RX) : origin=0x00001500 length=0x001FEB00
FLASH1 (RX) : origin=0x00200000 length=0x00200000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0007EB00
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
..\Debug\bl_src\Fapi_UserDefinedFunctions.obj (.text)
..\Debug\bl_src\bl_flash.obj (.text)
--library= F021_API_CortexR4_BE.lib < FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.SetActiveBank.obj
FlashStateMachine.InitializeFlashBanks.obj
FlashStateMachine.EnableMainSectors.obj
FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.ScaleFclk.obj
Init.obj
Utilities.CalculateEcc.obj
Utilities.WaitDelay.obj
Utilities.CalculateFletcher.obj
Read.MarginByByte.obj
Read.Common.obj
Read.FlushPipeline.obj
Read.WdService.obj
Async.WithAddress.obj
Program.obj > (.text)
} load = FLASH_API, run = RAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)
.text align(32) : {} > FLASH0 | FLASH1
.const align(32) : {} > FLASH0 | FLASH1
.cinit align(32) : {} > FLASH0 | FLASH1
.pinit align(32) : {} > FLASH0 | FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
}
5. I got bad function location which are in bl_flash.c. like this :
I will very appreciate for your help.
Best Regards!
Jinus
Hi Jinus,
1. You can find the sector information in the datasheet. Below is a snippet.
2. I think you need to use 150MHz instead. The 300MHz is for the CPU (GCLK) clock. However, the flash controller operates at half the frequency HCLK).
3. You should use F021_API_CortexR4_L2FMC_V3D16.lib or F021_API_CortexR4_L2FMC.lib
4. You need to replace with the correct library in your command file as indicated in 3) above.
5.
Hi Charles,
Thanks for your help, I have successful run uart bootloader and send bin file to lc4357. But, I've had some other problems.
1. Very time start user app form bootloader should goes to _c_int00(In user app, created by HalCogen 4.05). It seems that some configrations stop reinit cpu that will cause cpu Abort. If directly goes to main without doing cpu initialization in _c_int00, the app runs good without any problems.How to solve it?
2. How to create bin file that can download to interalflash directlly via uart port? I now using the tool hex470.exe. The hex file created by ccsv6 (Settings shows blow) is right?
Thanks!
Jinus.
Hi Jinus,
Please use the attached example. In the project property go to Steps under Build. See below screenshot. This is how I convert into a bin file.
7288.example_rtiBlinky_for_uart_bootloader.zip
Can you find out the cause of the abort by looking the DFSR (default fault status register) and DFAR (data fault address register) in the CPU?
Hi Charles,
Thanks very much. The bootloader for lc4357 runs well after using the bin file created by ccsv6.
Thanks again for your support.
Regards.
Jinus