Hello,
I was directed to post my problem here by customer service. I think the LAUCHXL2-RM57L that I received is defective. The XDS110 Status LED lights remain off when the board is plugged in. The board is not enumerated on the USB bus on two different computers. The out-of-box demo does not work. The Code Composer Studio cannot detect the board. The other development board that I received (MSP432P401R) has the same XDS110 debug interface and everything works perfectly. I have tried the basic troubleshooting steps such as replacing the USB cable and connecting to a different computer. The only LED that comes on is the +5V green LED when I connect the USB cable. Pressing any of the buttons on the board has not effect. I have tried to use the xdsdfu command line utility, but it does not detect anything on the USB bus when the Hercules launchpad is plugged in. The Hercules launchpad did not work from the first time that I plugged it in. Thanks.