From the safety perspective, RM46x series micro controllers seems to be well stuffed. We have some queries on the performance under harsh environments:
1. When we use these micro controllers in control systems in harsh industrial environments how is the reliability of these micro controllers? Like for example, if they are used in ECU in automobile industry, typical high vibration environments, what could be the affect on the micro controller assembled on the PCB?
2. Is there any certificate for these micro controllers tested under these scenarios mainly from the vibration scenario?
3. What specifications do these micro controllers comply with under vibration environments?
4. The scenario might be different if you use a BGA or QFN. What could be the choice among these for the RM46x for the automotive industry?