Hi,
one of my customers boards is using the TMS570LS3137 and right after POR_RST is released, the nRST gets driven low. The behavior is such the nRST really never goes high, so the TMS570 must be driving the nRST low very early on. There is a table in the TRM, Table 2-8 which describes the Reset Causes upon which the TMS570 is driving nRST low.
[] Are there any other causes where the MCU is driving nRST low outside of the table 2-8?
[] Which of the table 2-8 reasons would cause nRST to stay low, even after PORRST is released from reset? I.e. which reasons would occur very early on? Oscillator failure, Voltage Monitor ...?
[] Why could the nRST not rising?
Thanks,
--Gunter