hello everyone
I have the following problem which I couldn't solve so far:
for a project in my UNI I need to write a program which uses an external library in this case MPIR (Multiple Precision Integers and Rationals), following the instructions of the library; I built it using Microsoft Visual studio for generic c and got the files
1. Header: mpir.h
2.Library: mpir.lib
for the second step i need to run the code on my board Hercules RM57L843
1. I used HalCodGen to generate the required files
2. From ARM Compiler --> Include options -- I added the location of the library
3-1 ARM Linker--> File search Path --> at the top i added the location for the file mpir.lib
3-2 At the bottom I added again the location of the library folder.
4. when I build the project i get the errors:
error #10234-D: unresolved symbols remain
error #99923: Corrupt member header: 'C:/Users/masj/Documents/Code Composer/mpir-3.0.0/lib/Win32/Debug/mpir.lib'
if i remove 3-1 the former error (error #99923:) disappears.
My questions are:
1. How can I solve those errors.
2. Does it matter that the library was built using Visual Studio?
thank you
Sincerely
Moud