Other Parts Discussed in Thread: HALCOGEN, TMS570LS0432
Hi Team,
Recently, we have procured TMS570LS3137ZWT and started testing HET module using Code composer Studio 6.2 version.
Test case: We have configured in such a way that for pin 30 in NHET1 module, a square wave of 3 volts peak to peak is applied with 32 KHZ. We have configured NHET1 such that if the input frequency >=32 Khz, pin 31 should be set.
Observations:
1. With input frequency < 32 Khz with amplitude of the sampling signal is 3 Vp-p, pin 31 is not set.
2. With input frequency = 32 Kzh with amplitude of sampling signal is 3 Vp-p, pin 31 is set.
3. Now, we restarted the system and repeated step 1. Could see that pin 31 is set.
4. After step 2, we decreased input sampling signal amplitude to 500 mV and repeated step 1 and output is expected (pin 31 is not set).
5. After above step, we increased sampling signal amplitude to 3 Vp-p, still the pin 31 is not set (which is correct).
Problem: Once the pin is set, and after restart, with no change in sampling signal amplitude, always the pin is set.
Is it expected behaviour? How to overcome this?
Regards,
M.Sreenivasan.